CPT112S/CPT007B Capacitive Sense Profiler with ToolStick Base adaptor

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Master Employee</font></font> </a> delu on ‎04-13-2017 04:58 PM

Question

Does the Toolstick Base Adapter support Capacitive Sense Profiler with CPT112S/CPT007B devices?

Answer

Yes, you can connect the base adapter and CPTxxxx device through C2 interface.

Take the CPT112S STK as example, the connection is depict as below:

 C2_CPT112S.png

The schematic of the ToolStick Base Adapter is available in this document (page 5).

 

The pins for the CPT112S EXP are shown in the picture below:

 

CPT112S.png