CP2114 LRCLK Frequency

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Jiehui on ‎10-30-2016 10:22 PM

Question

What is the max. LRCLK frequency supported by CP2114?

Answer

The CP2114 supports only 48 kHz digital audio. This is typically not an issue for source USB audio as the device capabilities are reported to the host and any sample rate conversion (for say 44.1 kHz audio) is done automatically by the host.