Reply
Posts: 2
Registered: ‎11-28-2016
Accepted Solution

Si86IsoLin DC Capabilities

Could the Si86IsoLin kit handle DC to 80Hz input? The kit include 3 isolation chips. The resolution of each chip is different. The chips are supposed to handle high frequencies. But I am not sure if it handles low frequencies well.

Posts: 2
Registered: ‎11-28-2016

Re: Si86IsoLin DC Capabilities

I found out. The answer is yes. The iso-chips can handle DC to 80 Hz.

 

http://www.mouser.com/ds/2/368/AN559-737731.pdf