Reply
Posts: 48
Registered: ‎11-07-2015
Accepted Solution

Qualifiers for community's ranks

On page with ranks http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Pr... there aro no qualifiers for each rank.

 

Maybe add qualifiers will be good feature?

 

For example:

For reach a rank "Hero" you need post XXX messages, get YYY kudoes, etc.

_____________________
Best regards,
Danil Borchevkin,
Owner Lab409.ru
Highlighted
Administrator
Posts: 676
Registered: ‎09-04-2012

Re: Qualifiers for community's ranks

Hi, @DanilBorchevkin

 

Good question. When we set up the ranking system, we followed some best practice tips from our platform provider. One of the recommendations was not to share the rank structure with users to avoid some users to "game the system" to attain higher ranks. For example, they may be able to give kudos to any post etc. 

 

I see that it can be motivating for users to view a status bar showing progress towards the next rank though.  


Nari | Community Manager | Silicon Labs