Statement of Volatility

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Silicon_Labs on ‎12-11-2013 03:31 PM - edited on ‎02-20-2017 04:39 AM by Administrator Siliconlabs
Question

 

My project requires a Statement of Volatility before I can use a Silicon Labs MCU. Where can I obtain a Statement of Volatility for a given MCU?




Answer

 

A Statement of Volatility can be obtain by contacting Silicon Labs technical support: http://www.silabs.com/support/resources

The Statement of Volatility we provide is signed and contains the following information:

  • Amount of volatile memory (if any)
  • Amount of non-volatile memory (if any)
  • Procedure to sanitize/erase non-volatile memory (if applicable)

If you require any additional information in the Statement of Volatility, be sure to specify the requirements when contacting technical support.