Can the Si86xx have 2.5V on one side and 5V on the other side? Can I use it as a level shifter?

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Silicon_Labs on ‎05-02-2017 08:09 AM - edited on ‎07-25-2017 01:59 PM by Administrator Siliconlabs

Question

Can the Si86xx have 2.5V on one side and 5V on the other side?  Can I use it as a level shifter?

Answer

Yes, internally the Si86xx has two independent dies that are each powered separately.  Either die can be powered from 2.5V to 5.5V.

 

Learn more about the Si86xx isolators: http://www.silabs.com/products/isolation/digital-isolators/si86xx-digital-isolators