Reply
Administrator
Posts: 672
Registered: ‎09-04-2012

Show us your summer project for a chance to win a free Basis watch!

[ Edited ]

show us your summer project.png

 

What project are you working on this summer? A low-power game module run by the EFM32 microcontroller? A touchless optical switch using the Si114x sensor? Or a Rube Goldberg machine connected via the EM357 ZigBee chip?

 

Whatever it is, share your cool project with your fellow engineers here by posting a photo of your project using a Silicon Labs' part and a short description of what it is in the comments below. We’ll pick three best photos based on most kudos (50%) and a voting system by our in-house judges (50%). The winners will receive a free PEAK™ (Matte Black / Black, $199.99).

 

In order to be eligible, your entry must meet the following requirements:

  • Image file types allowed: gif, jpg, jpeg, png
  • Silicon Labs’ product or software tool needs to be depicted in the photo.

 

Your entry will be judged by three or more employees of Silicon Labs and will be judged based on

  • Creativity
  • Quality of presentation

 

Number of winners: 3 (only one entry per user) 

Prize: 1 x PEAK™ (Matte Black / Black, $199.99)

Contest period: 27 July, 2015 – 21 August, 2015

 

By entering the contest you acknowledge that you have read and agree to the Community Contest Terms and Conditions 


Nari | Community Manager | Silicon Labs
Posts: 4
Registered: ‎08-06-2015

Re: Show us your summer project for a chance to win a free Basis watch!

so WHERE to post?

Administrator
Posts: 672
Registered: ‎09-04-2012

Re: Show us your summer project for a chance to win a free Basis watch!

[ Edited ]

Hi, @antti you can post an image in the comment. 

 

1669921_597681396977217_1897373980_o.jpg


Nari | Community Manager | Silicon Labs
Posts: 2
Registered: ‎08-12-2015

Re: Show us your summer project for a chance to win a free Basis watch!

Software Defined Radio for the Ham bands, using Silicon Labs Si570 and PSoC.

 

Si570 based SDR

 

See also this video:

Posts: 4
Registered: ‎08-12-2015

Re: Show us your summer project for a chance to win a free Basis watch!

I assembled a mini weather station with wireless temperature and humidity sensor. The receiver chip is Si4362 and the display shows alternating outside temperature/humidity along with the transmitter battery status and atmospheric pressure in mmHg units. The scrolling pressure graph is updated every 15 minutes and holds pressure history for the last 25 hours. The receiver is powered from a wall adapter, but has a rechargeable battery on board. Average current consumption is about 0.7mA in standby (because of LCD) and around 13 mA when receives data from the transmitter.

schema_RX.png

 rx1b.jpg    rx2b.jpg  rx3b.jpg

 

The transmitter unit uses Si7021 sensor and is build around Si4060. It is mounted outside in a PVC pipe, transmits temperature/humidity data every minute on 916 MHz band, and serves a similar receiving device as above at our neighbors. It is powered from XENO lithium battery and enclosed into a box from Radioshack. Average current consumption is about 10 uA. Previously constructed system based on CC1101 transmitters survived 2 last brutal Wisconsin winters and runs from such battery already for over 2 years.

schema_TX.png

 

tx1.jpg   tx2.jpg  tube1.jpg

Posts: 2
Registered: ‎08-13-2015

Re: Show us your summer project for a chance to win a free Basis watch!

I haven't started a project yet but I have got the samples

 

Maybe I can have a chance to win, who knows Robot Happy

 

reading the datasheet of #Si1102, this is the biggest step of a project Robot Happy

 

https://twitter.com/argenindelisi

 

si1102.jpg

Posts: 71
Registered: ‎06-17-2014

Re: Show us your summer project for a chance to win a free Basis watch!

Hi!

I'm currently working on a indoor unit for my weather station mesh network. 

Weather Station project:

http://community.silabs.com/t5/Projects/Weather-Station-Mesh-Network/m-p/151966#U151966

 

inside_unit_edit.jpg

 

There is one weather station located in my garden, which broadcasts the data to all participants of a ZigBee network. The coordinator of the network operates as base station and passes the data on to a web-server, which displays the data in a chart. However if I want to know something about the weather data, I need a smartphone or a PC. So I decided to build a so called "indoor unit". These devices will consist of a TINY GECKO MCU, a XBee S2 radio, a 7-segment LCD (similar to the one on the TG STK) and a coin cell battery. The ZigBee radio will operate in a cyclic sleep mode and therefore join the mesh network as an end-device. It will wake up every ten minutes and check if the coordinator has new data available. If there is new data, the MCU will be woken up due to a LEUART interrupt and update the display.

Some improvements for the future would be a temp/humidity sensor for each "indoor unit" and a energy harvesting system to power it from indoor light. 

 

Kind Regards,

Michael

 

 

Posts: 10
Registered: ‎03-26-2013

Re: Show us your summer project for a chance to win a free Basis watch!

I'm currently working on a project to make a scrolling display controlled by Zero Gecko Starter Kit. The scrolling display is used to give status update of a test. The scrolling display is used  to display date, time and temperature  (see video in the attachment).

Posts: 2
Registered: ‎08-13-2015

Re: Show us your summer project for a chance to win a free Basis watch!

Today is 21 August, who is the winner Robot Happy 

 

 

Posts: 2
Registered: ‎08-12-2015

Re: Show us your summer project for a chance to win a free Basis watch!


ZerOne wrote:

Today is 21 August, who is the winner Robot Happy 

 

 


 

I think they will wait for more kudos.

I voted for sergeilb and michael_k.

 

Gerrit.

Highlighted
Administrator
Posts: 672
Registered: ‎09-04-2012

Re: Show us your summer project for a chance to win a free Basis watch!

Thanks for sharing your projects with us! We hope you had a wonderful summer and had some fun with your project Robot wink

 

The winner of the summer contest goes to…

 

@soldeerridder - Software Defined Radio for the Ham bands

@sergeilb - A mini weather station with wireless temperature and humidity sensor

 

We look forward to learning more about the project. It would be great if you can share more details on the project page Robot Happy 

 

@michael_k - Weather station mesh network

Thanks for sharing your weather station project on the project page, Michael! Can't wait to see the module with the ZigBee radio!

 

Congratulations! You will receive a private message about shipping information soon.

 

Cheers,

Nari


Nari | Community Manager | Silicon Labs