Reply
Highlighted
Posts: 164
Registered: ‎09-17-2012

[DC12-S2-11] Geckolizator

[ Edited ]

Geckolizator

To help to protect owners' cars I have designed the device based on GPS/GSM localization. When the car has clear sky view it would get a geolocation fix via GPS and when GPS signal is not available, the pinpoint position would be established based on GSM base stations only, since GSM signal penetrates through buildings. In urban areas a GSM based location fix accuracy is about tens to hundreds meters and in country sides it is more likely to be kilometers. Still, it is a good starting point for the police to find your stolen vehicle.

The system overview is presented in pictures below.

GL_1.JPG

GL_2.JPG

GL_3.JPG

The Geckolizator is a battery operated device (Li-Po 1500mAh cellphone battery). It also has battery charger implemented. This is the 5V/500mAh MAX1811 USB charger. When the car engine is turned on and the 12V is available in the car, the device recharges battery using 12V/5V car adapter. What you do with Geckolizator is you hide it somewhere in your car and connect it to this 12V/5V adapter. When you leave your car in non secure location (or even in your garage), always arm it (turn on). The system will initialize the accelerometer (MMA7455L) and go into EM3 mode. EM4 could have been used, but I could not find EM4 wakeup pins on EXP, so I have used EM3. Now, when someone manages to steal your car and drives it off, accelerometer generates interrupt. EFM wakes up, turns off accelerometer and turns on HOPE's GPS reveiver (GPS03) and Sagem's HiLo GSM/GPRS modem. Now, when GPS signal is valid after a few seconds, the system sends SMS with localization data. If the GPS signal is not valid (not clear sky view and when your car is already inside a truck Robot Happy heading somewhere), the Geckolizator uses GSM base stations signal to check the possible location with a use of Google's databases and also sends you SMS. Then EFM turns off GSM modem, but leaves GPS receiver to maintain signal availability or to get a fix which was not available then and EFM goes to EM2 for a programmed time (in the demo, it is 5 minutes). After this time it wakes up and starts localization scheme one more time and sends sms. This is being done until you turn off the device, there are no more money on SIM prepaid card or battery drains out. EM4 with GG can also be used for timed wakeup.

eA.png

Why I have used EFM? When you do not use your car very often, you do not want to drain your car battery (especially in winter) if you have 12V in your connector when engine is off. In the same time you want to keep your car safe and monitored by Geckolizator. That is why EFM are the perfect fit for this design in my opinion.





GL_4.JPG



TODO list:

  • Implement EFM on Geckolizator to get rid off STK in the car

  • Change GPS enable MOS for low power switch


    Attached Files

Posts: 556
Registered: ‎05-14-2012

[DC12-S2-11] Geckolizator

Thank you for joining stage 2 of the contest and sharing your design. Below are a few comments from the jury:

Interesting project that I'm sure would give many people some peace of mind when they leave their car unattended. Could even be adapted to bicycles for example. Then energy optimization becomes even more important. This project also demonstrates the need for low power accelerometer and gps devices.

Very smart to have both GPS and GSM localization. The working demo is very cool and it is good that you have implemented a char charger so you can always have the device in your car.

The idea itself is not novel, but a nice implementation. The question is whether it is necessary to connect it to the car battery at all, as the device seems only to be using the GPS and the GSM when it is stolen. This limited use could be run from batteries I think. When using the car normally I guess it should be disarmed anyways, as you otherwise would get lots of text messages all the time. Without batteries it would also be easier to fit it wherever you wanted to in the car, and thereby also harder for the thief to predict where it can be. Great also with the positive externalities of these systems.
Posts: 164
Registered: ‎09-17-2012

[DC12-S2-11] Geckolizator

Thanks for the kind words.

I connected the device to the car battery, but it is not visible. Extra pair of 12V cables were led under car carpet so everything is out of reach for eyes Robot Happy
Posts: 68
Registered: ‎09-16-2012

[DC12-S2-11] Geckolizator

Wow! Your Geckolizator (unfortunately with name changed) is on Hack a Day!

http://hackaday.com/2013/02/13/roll-your-own-lojack-clone/

Congratulation!
Posts: 164
Registered: ‎09-17-2012

[DC12-S2-11] Geckolizator

Thanks!
Posts: 556
Registered: ‎05-14-2012

[DC12-S2-11] Geckolizator


Sebastian wrote:

Wow! Your Geckolizator (unfortunately with name changed) is on Hack a Day!http://hackaday.com/2013/02/13/roll-your-own-lojack-clone/Congratulation!




Cool stuff Gelmi. Congratulations!
Posts: 4
Registered: ‎02-15-2013

[DC12-S2-11] Geckolizator

Nice project !

It would be great to use energy harvesting in this project. (but hard with the GSM)

I would try, bu not way to find a sample of the EFM32 board ...
Posts: 256
Registered: ‎09-07-2012

[DC12-S2-11] Geckolizator

The starter kit? It can be bought from Digikey, for example: http://www.digikey.com/product-search/en?lang=en&site=us&KeyWords=stk3700&x=0&y=0
Posts: 556
Registered: ‎05-14-2012

[DC12-S2-11] Geckolizator

Posts: 164
Registered: ‎09-17-2012

[DC12-S2-11] Geckolizator

...or be creative at the next EFM32 Design Contest Robot Happy
Posts: 4
Registered: ‎02-15-2013

[DC12-S2-11] Geckolizator

In facts, my company asked for a kit on the energymicro website and never had news about it.
Posts: 119
Registered: ‎05-30-2012

[DC12-S2-11] Geckolizator


jujun wrote:

In facts, my company asked for a kit on the energymicro website and never had news about it.




Let's have a look at the procedures. The distributor partners are not obliged to give away free kits, as stated, but a reply should be given after registration for sure.
Posts: 73
Registered: ‎09-24-2012

[DC12-S2-11] Geckolizator

Perfect!

Are you plan to publish software on github ?
Posts: 164
Registered: ‎09-17-2012

[DC12-S2-11] Geckolizator

I think yes, but I have to make this code 'usable' for you, because I got my PCBs just 6 days before submission deadline, so I had very little time to solder everything and create the code that works and also to make youtube video Robot Happy So I have made too few comments in code to make it easy to read. When I find some free time to make the code readable - at least in some way, I will upload the code somewhere and let you guys know.

Are you interested in any particular part of the code?
Posts: 73
Registered: ‎09-24-2012

[DC12-S2-11] Geckolizator

Yes - may be some parts may be helpfull.
Posts: 79
Registered: ‎08-10-2012

[DC12-S2-11] Geckolizator

Gelmi,

you should consider adding a Solar Panel charger. This allows you to add this device to equipment that has no power source and tracking it.

E.g. on top of a container.

/Mads
My views are my own and do not necessarily represent the views of Silicon Labs
Posts: 164
Registered: ‎09-17-2012

[DC12-S2-11] Geckolizator

I thought about it. That is why I chose MAX1811 as a charger - input up to 6,5 V. So, I believe I could add 6V solar panel only with a diode and MAX1811 would still control charging process.