回复
发帖数: 1
注册日期: ‎08-24-2017

si4463 match no interrupt

my config:

 SI446x_Set_Property_1(MATCH_VALUE_1, 0x31);
SI446x_Set_Property_1(MATCH_MASK_1, 0xFF);
SI446x_Set_Property_1(MATCH_CTRL_1, 0x40);
#define RF_INT_CTL_ENABLE_4 0x11, 0x01, 0x04, 0x00, 0x07, 0x98, 0x01, 0x08

it means: //INT_CTL_PH_ENABLE - 0x98, enable MATCH interrupt.

i read GET_INT_STATUS;;;return FF 00 04 00 02 00 00 10 14  it means:

FILTER_MATCH = 0,FILTER_MISS=0,PACKET_SENT=0,PACKET_RX=0.

????????????????????????????????????????????????????????

发帖数: 94
注册日期: ‎12-02-2016

Re: si4463 match no interrupt

Hi,

Please check if the configuration of TX side is fine. Frequency, channel, datarate, deviation, packet configuration, the first byte in the payload, etc.

I've checked on our DK, the match function and the corresponding interrupt works well. So, please check your rx and tx configuration carefully first.

 

Regards,

Yongsheng