回复
发帖数: 14
注册日期: ‎08-15-2016

SI4464有没有C2A版本的芯片?是不是SI4464没有打算升级到C2A版本?

现在的4464B1B版本感觉好多细节不好,4463的C2A版本就好很多,不知道SI4464是否会出C2A版本?

发帖数: 251
注册日期: ‎12-10-2013

回复: SI4464有没有C2A版本的芯片?是不是SI4464没有打算升级到C2A版本?

There is no plan to update to next version for si4464. Some frequency bands which are covered by si4464 is already covered by si4463 C version chip.

 

 

Juanyong

发帖数: 1
注册日期: ‎08-04-2017

回复: SI4464有没有C2A版本的芯片?是不是SI4464没有打算升级到C2A版本?

SI4463-C2A没有覆盖SI4464-B1B的全部频段,比如230MHz和280Mhz,期待SI4464升级。SI4464-B1B在发送超长数据时,比如2000+Byte,FIFO逻辑无响应,存在问题

Highlighted
发帖数: 14
注册日期: ‎08-15-2016

回复: SI4464有没有C2A版本的芯片?是不是SI4464没有打算升级到C2A版本?

4463的频段覆盖比4464少很多。 B1B版本很多细节部分不好,真的非常期待4464能够升级到C2A版本。