回复
发帖数: 5
注册日期: ‎09-14-2017

SI4463通信频率在250K时发一会死机

安装软件配置的程序,一对一目前在调试,通信频率在100K时正常,250K时发一会发送端就死机,求高人指点!万分感谢!

发帖数: 101
注册日期: ‎12-02-2016

Re: SI4463通信频率在250K时发一会死机

Hi,

Could you give more detailed information about the test process?  Is the test bidirectional communication? What's the mcu / radio state when the communication halts?


Regards,
Yongsheng
发帖数: 5
注册日期: ‎09-14-2017

Re: SI4463通信频率在250K时发一会死机

您好!

我程序写了发送和接收子函数,通过串口命令控制接收和发送状态。一个设置为接收,另一个设置为发送。发送的长度为50个字节,在接收完一个数据包之后读取中断并清除中断,并且清除接收FIFO寄存器的值。 SI4463的频率为433Mhz,当RF速率为100K时,接收正常。当RF速率为250K时,发送一会就死机了。

发帖数: 5
注册日期: ‎09-14-2017

Re: SI4463通信频率在250K时发一会死机

您好!

我程序写了发送和接收子函数,通过串口命令控制接收和发送状态。一个设置为接收,另一个设置为发送。发送的长度为50个字节,在接收完一个数据包之后读取中断并清除中断,并且清除接收FIFO寄存器的值。 SI4463的频率为433Mhz,当RF速率为100K时,接收正常。当RF速率为250K时,发送一会就死机了。MCU采用的是STM8L103.

发帖数: 101
注册日期: ‎12-02-2016

Re: SI4463通信频率在250K时发一会死机

1. Please check what the mcu and radio status are when the communication halts. Check out if rx breaks or tx breaks, and check out if mcu breaks or radio breaks.
2. Have you tested the hardware performance by using RF instruments? If not, please test it first, including tx power / frequency error / rx sensitivity.

By the way, could you send us your radio configuration files (XML file which is produced by WDS) about 100kbps and 250kbps?   We would review it to see if there's obvious problem about the configuration.

Regards,
Yongsheng
Highlighted
发帖数: 5
注册日期: ‎09-14-2017

Re: SI4463通信频率在250K时发一会死机

好的,非常感谢您!我将继续修改调试。抱歉上一个回复错误,是接收端挂死。目前调试能运行一个多小时。我把我工程的放在附件中,麻烦您给指导下!万分感谢!