回复
发帖数: 22
注册日期: ‎08-16-2017

IEEE 802.15.4 and RAIL/Flex SDK

示例工程里面没有采用IEEE 802.15.4通信协议的工程啊?要怎么配置才能采用这个协议通信呢?

发帖数: 22
注册日期: ‎08-16-2017

回复: IEEE 802.15.4 and RAIL/Flex SDK

好吧!论坛是如此的冷清,我自己在railtest模板工程里添加了802.15.4协议相关配置函数,现在已经正常工作了。按照文件提供的说明就可以了。

发帖数: 94
注册日期: ‎12-02-2016

Re: IEEE 802.15.4 and RAIL/Flex SDK

Hi,

I think you need to read the guide documents about Flex. They're located under Flex's stack diretory.

About this question, it's suggested to use railtest for a general evaluation. One of the documents introduces railtest.

Below is the directory of the railtest document in my computer, yours should be similar.

file:///C:/SiliconLabs/SimplicityStudio/v4/developer/stacks/flex/v1.0.1.0/protocol/flex_1.0/documentation/RailTestUserGuide.html

 

By the way, if you have some urgent issues, please contact our distributor or salesman or FAE, and ask them for helping create the normal salesforce tictket, we usually deal with the salesforce ticket in a high priority.

 

Regards,

Yongsheng

发帖数: 22
注册日期: ‎08-16-2017

Re: IEEE 802.15.4 and RAIL/Flex SDK

非常感谢!我已经在例程的基础上成功实现了IEEE 802.15.4的通信协议了,用户手册的确很重要。

发帖数: 2
注册日期: ‎08-07-2017

Re: IEEE 802.15.4 and RAIL/Flex SDK

如何实现的?