回复
发帖数: 1
注册日期: ‎04-18-2017

Can I generate a Green Power Source Node Use the ember chips

Hi, now I have a question about the green power, can i use ember chips (such as em3585) to make a Green Power Source Node? And how to do this.

Thanks for your reply!

发帖数: 75
注册日期: ‎04-26-2016

回复: Can I generate a Green Power Source Node Use the ember chips

Hello,

 

Regarding the GreenPower, it is about the software, so you can use EM35x chip or EFR32 chip, there is no restrict on the hardware.

 

You can use the Z3 Gateway (which has Green Power proxy feature) and the Z3 Light (which has Green Power sink feature) sample apps. Under AppBuilder Plugins tab, note the "Green Power Library" and a number of "Green Power *" plugins. You can look up our App Framework API Reference (120-3023-000_AF_V2_API.pdf) for green power related APIs.

 

I recommend to setup sample with CLE EM3588 module firstly, and then you can create a project for EM3585 base on the board header file from EM3588 project.

 

Best Regards,

Lei

 

 

发帖数: 75
注册日期: ‎04-26-2016

回复: Can I generate a Green Power Source Node Use the ember chips

Hello,

 

Regarding the GreenPower, it is about the software, so you can use EM35x chip or EFR32 chip, there is no restrict on the hardware.

 

You can use the Z3 Gateway (which has Green Power proxy feature) and the Z3 Light (which has Green Power sink feature) sample apps. Under AppBuilder Plugins tab, note the "Green Power Library" and a number of "Green Power *" plugins. You can look up our App Framework API Reference (120-3023-000_AF_V2_API.pdf) for green power related APIs.

 

I recommend to setup sample with CLE EM3588 module firstly, and then you can create a project for EM3585 base on the board header file from EM3588 project.

 

Best Regards,

Lei