回复
发帖数: 22
注册日期: ‎08-16-2017

在使用flex gecko的板子,工程里有些配置不太理解,请各位大侠帮我看看

大家好!我有些问题想请教,如下:

1、base channel frequency:开始频率

2、channel spacing            :通道间的频率间隔,通道号加n,其对应的频率就是

                                             base channel frequency + (channel spacing) * n , 是这样吗?

3、bitrate                            :发送速率,也就是通信带宽?

4、deviation                        :频偏,要怎么设置?

5、baudrate tolerance        :波特率的PP值,要怎么设置?

 

不知道理解的对不对,

发帖数: 22
注册日期: ‎08-16-2017

回复: 在使用flex gecko的板子,工程里有些配置不太理解,请各位大侠帮我看看

这的频偏是不是就是载波带宽?我是这么理解的,不知道对不对?

发帖数: 94
注册日期: ‎12-02-2016

Re: 在使用flex gecko的板子,工程里有些配置不太理解,请各位大侠帮我看看

Hi,

1、base channel frequency:开始频率
A:     Yes, it is.  It's channel 0.
 

2、channel spacing            :通道间的频率间隔,通道号加n,其对应的频率就是

                                             base channel frequency + (channel spacing) * n , 是这样吗?
A:    Yes, it is.

 

3、bitrate                            :发送速率,也就是通信带宽?
A:    No,  it's data rate.

4、deviation                        :频偏,要怎么设置?
A:  Usually, it should refer to the specific standard or regulations.  For a completely customized product, it's suggested to set it with half of the data rate /  bitrate.

5、baudrate tolerance        :波特率的PP值,要怎么设置?
A:  It's based on your real application, such as data rate, frequency error or crystal accuracy, and the maximum length of the packet.
      For the low data rate, usually set it with 0.   For the high data rate, if the communication is unstable, you should set it with a proper value.


Regards,
Yongsheng

Highlighted
发帖数: 22
注册日期: ‎08-16-2017

Re: 在使用flex gecko的板子,工程里有些配置不太理解,请各位大侠帮我看看

谢谢你的帮助,现在明白了!