Reply
Highlighted
Posts: 5
Registered: ‎02-23-2016

The Wizard Gecko WGM110 Wi-Fi module is here!

WGM110 is the Easiest Path to Native IoT.

 

Press Release: http://news.silabs.com/press-release/product-news/silicon-labs-simplifies-wi-fi-connectivity-plug-an...

 

WGM110 Page: http://www.silabs.com/products/wireless/wi-fi/wi-fi-modules/Pages/wgm110-wi-fi-module.aspx

 

The Silicon Labs Wizard Gecko WGM110 Wi-Fi module is targeted for applications where leading RF performance, low power consumption and fast time to market are key requirements.

 

The WGM110 integrates all elements required to build a Wi-Fi IoT device; including a 802.11b/g/n radio, integrated antenna, certifications, a microcontroller, Wi-Fi and IP stacks, an HTTP server and multiple protocols such as TCP and UDP along with end-to-end security with TLS/SSL.

 

WGM110 can host BGScript end user applications or be used in Network Co-Processor mode together with an existing customer MCU.

 

Discover Wi-Fi and the WGM110 Wi-Fi module and enter the easiest path to native IoT.

 

Get started by ordering the WGM110 Wireless Starter Kit and download the free Wizard Gecko SDK from www.silabs.com/start-wgm

Posts: 63
Registered: ‎04-14-2015

Re: The Wizard Gecko WGM110 Wi-Fi module is here!

I know exactly what to do with these next Christmas. Robot Happy
Posts: 2,638
Registered: ‎08-25-2015

Re: The Wizard Gecko WGM110 Wi-Fi module is here!

@mapleleafs Why not start right-away? Smiley Wink

Posts: 63
Registered: ‎04-14-2015

Re: The Wizard Gecko WGM110 Wi-Fi module is here!

Well if you really wanted to go all out--do a Trail of Lights display worthy of Zilker park--right away might be more appropriate. The way I would do it would use around 8 WG boards. What I would use the WiFi for...I'm not saying on a public board. :-p
Posts: 56
Registered: ‎01-29-2016

Re: The Wizard Gecko WGM110 Wi-Fi module is here!

Just a little size reference:

WGM110_Front.JPG

WGM110_Back.jpg