Reply
Posts: 238
Registered: ‎10-03-2015

Setting Tx Power on-the-fly

Is it safe / effective to set Tx power during a connection open event (gecko_evt_le_connection_opened_id)? I am thinking no, but I'd like to have the BGM's Tx power as low as possible until a connection is made then increase it to ensure the best connection performance possible. 

 

Is the above sensible / possible?

 

 

Posts: 2,638
Registered: ‎08-25-2015

Re: Setting Tx Power on-the-fly

Hi,

 

 

Not according to the API Guide:

 

NOTE: This command should not be used while advertising, scanning or during connection.

 

Regards,

Tiago

Highlighted
Posts: 238
Registered: ‎10-03-2015

Re: Setting Tx Power on-the-fly

Sorry, I should have mentioned that I saw that note and that is what prompted my question in the first place. Since I am attempting to conserve power while advertising and disconnected AND achieve the best possible RF performance while connected I was wondering if there was a strategy to manipulate the TX power dynamically to do this....or if it's even worth the effort.

 

If I must avoid using this function when a connection opens then perhaps I can use a connect / reconnect process that sets the TX power and then returns to the lower TX power upon the a subsequent disconnect.