Reply
Highlighted
Posts: 2
Registered: ‎02-01-2016

Power on start BLE121LR

[ Edited ]

Hello!

 

I performed all the necessary connections to connect the BLE121LR module, however I can not find it to pair with your phone. Can someone help me?

 

The connections I made were:
3V3 - AVDD
3V3 - VDD
GND - All GND
RESET - NC

 

Module is consuming + or - 8 mV.

 

thank you

Posts: 2,220
Registered: ‎08-25-2015

Re: Power on start BLE121LR

Hi,

 

Are you running one of the SDK's BGScript examples?

 

Regards,

Tiago

Posts: 2
Registered: ‎02-01-2016

Re: Power on start BLE121LR

I'm not using any software, just did the power connections to run the module.

It does not come from the factory no settings where I put energy into it and it works?

thank you

Posts: 2,220
Registered: ‎08-25-2015

Re: Power on start BLE121LR

Hi,

 

No, these are the factory settings. It essentially comes with BGAPI access via UART so unless you hook it up to a host (microcontroller, PC) and send a couple commands it will just go to PM3.

 

Regards,

Tiago