Reply
Posts: 5
Registered: ‎08-03-2017

No BGSCRIPT examples in SImplicity Studio install

Hi

I have a BGM development kit, I have installed SImplicity Studio and the BLE SDK. However, there I don't see any BGSCRIPT example folders.

 

I followed this post:

http://community.silabs.com/t5/Bluetooth-Wi-Fi-Knowledge-Base/How-to-install-BLE-SDK-2-0-0/ta-p/1788...

 

But there is no "stacks" folder in C:\SiliconLabs\SimplicityStudio\v4\developer

 

I have logged into Simplicity Studio with my community account.

 

Thanks

Posts: 2,724
Registered: ‎09-01-2015

Re: No BGSCRIPT examples in SImplicity Studio install

Which version of the SDK did you install? BGScript support was announced deprecated some time ago and BGScript tools/examples were removed from the SDK starting from version 2.4.0.

 

I strongly suggest you start working with C as BGScript is no longer under active development. You can use the free GNU toolchain to build your projects, all the required development tools are free of charge.

Posts: 94
Registered: ‎12-07-2016

Re: No BGSCRIPT examples in SImplicity Studio install

Does this apply to the WGM110 as well?  Is there a C SDK available for it?

 

Thanks,

 

Scott

Posts: 2,724
Registered: ‎09-01-2015

Re: No BGSCRIPT examples in SImplicity Studio install


madsci wrote:

Does this apply to the WGM110 as well?  Is there a C SDK available for it?

 


No, this applies only to BLE SDK. There is no C SDK for WGM110.

Posts: 94
Registered: ‎12-07-2016

Re: No BGSCRIPT examples in SImplicity Studio install

Ok, thanks.  I'm not using BGSCRIPT there for anything more than reporting a version number anyway.

 

Scott

Posts: 5
Registered: ‎08-03-2017

Re: No BGSCRIPT examples in SImplicity Studio install

If there's no more support for BGSCRIPT, how do I use SPI with BGM111?

 

The only example I see for SPI is based on BGSCRIPT:

 

http://community.silabs.com/t5/Bluetooth-Wi-Fi-Knowledge-Base/BGM111-SPI-bit-bang-example-using-devk...

 

Thanks

Posts: 2,724
Registered: ‎09-01-2015

Re: No BGSCRIPT examples in SImplicity Studio install

We have a C-based SPI example for BGM111, see following KB article:

http://community.silabs.com/t5/Bluetooth-Wi-Fi-Knowledge-Base/Using-accelerometer-found-in-the-WSTK-...

 

The "bit bang" SPI implementation you linked was just kind of an ugly workaround because BGScript does not have SPI support. With C based apps you can use USART peripheral for SPI transfers which makes it much more efficient.