Reply
Posts: 28
Registered: ‎09-09-2015

Make it Small, Make it Fast, Make it First: Introducing the World’s Smallest Bluetooth Module

We know designers face a host of stressful design challenges, day in and day out, as well as the never-ending rush to get their products to market ahead of the pack. That’s why we’re always genuinely excited when we can release truly cutting-edge, industry-first innovations that can help our customers — innovations such as our new BGM12x system-in-package (SiP) module.

 

Ultimately the industry’s smallest Bluetooth low-energy SiP module with an integrated antenna, the BGM12x offers designers a way to finally effectively miniaturize many IoT applications in a manner that’s both cost-effective and doesn’t compromise on performance. We think the BGM12x is poised to help lead innovations in many application types, including sports and fitness wearables, smartwatches, personal medical devices, wireless sensor nodes, and other space-constrained connected devices.

 

SiP_Ruler.png

 

One of the biggest benefits of the BGM12x is simply helping vent pressures on designers by helping lessen the traditional development cycle thanks to the integrated antenna, radio, MCU, and software stack. With the BGM12x, engineering departments don’t have to spend any time on antenna design and certification testing. And quite simply, there is nothing else on the market with the size and performance combination that includes a high-performance antenna and an always up-to-date Bluetooth stack together. On top of this, designers get to utilize the favored ARM Cortex-M4 processor.

 

Additionally, there is just the overall benefit that using a wireless module reduces design time and long-term costs by lowering risks. With a proven, ready-to-go system, designers can skip complex RF design and move on to adding value to their core applications – what meaningful IoT development is all about anyway. And the exceptionally small size makes it very easy to use in two-layer PCB designs where board clearance continues to remain a critical concern.

 

We’re also happy that like all our Blue Gecko modules, designers can begin with a module-based design but easily migrate to a Blue Gecko SoC with minimal system redesign and full software reuse because of very similar technical features and identical APIs. Again, it’s about giving designers huge time savings, flexibility, and reduced headaches in the long term and helping work seem more a labor of love vs. going down a rabbit hole of chaotic alternatives.

 

 Screen Shot 2016-11-08 at 7.50.37 AM.png

 

And speaking of flexibility, we’re also excited that BGM12x is supported by our efficient wireless software development kit (SDK) that gives designers the ability to use either a host or fully standalone operation with BGScript. Our Bluegiga BGScript tool lets designers create Bluetooth applications quickly without using an external MCU to run the application logic, ultimately reducing system cost, board cost, and time to market as well.

 

BGM12x Features Overview:

  • Best-in-class SiP module size: 6.5 mm x 6.5 mm x 1.5 mm
  • Integrated chip antenna with exceptional RF performance (70% antenna efficiency) and an RF pad option for connecting to an external antenna
  • Output power: +3 dBm to +8 dBm supporting ranges from 10 meters to 200 meters
  • Based on Silicon Labs’ Blue Gecko SoC combining a 2.4 GHz transceiver with a 40 MHz ARM Cortex-M4 processor core and 256 kB flash and 32 kB RAM
  • Energy-efficient Bluetooth solution consuming 9.0 mA (peak receive mode) and 8.2 mA @ 0 dBm (peak transmit mode)
  • Hardware cryptography accelerator supporting advanced AES, ECC and SHA algorithms
  • Industry-proven Silicon Labs Bluetooth 4.2 stack with frequent feature enhancements
  • Rapid time to market with global RF certifications
  • Easy-to-use development tools: Simplicity Studio, Energy Profiler, BGScript
  • Worldwide application engineering support
Posts: 268
Registered: ‎02-20-2016

Re: Make it Small, Make it Fast, Make it First: Introducing the World’s Smallest Bluetooth Module

Very cool! 

Congratulations on the miniature size. 

 

Are there any major differences with the BGM111 aside from the RX sensitivity and size?

(I could not find many) 

Posts: 28
Registered: ‎09-09-2015

Re: Make it Small, Make it Fast, Make it First: Introducing the World’s Smallest Bluetooth Module

 

Hi,

 

Thanks. We are pretty exited about this product as well. 

 

The major differences to BGM111 are:

+ Smaller size

+ Few more I/Os available

+ RF pin option available

- Lower sensitivity

- No South-Korea certification and limited FCC certification, so a few 
more FCC test cases need need to be done for the end product

Posts: 28
Registered: ‎09-09-2015

Re: Make it Small, Make it Fast, Make it First: Introducing the World’s Smallest Bluetooth Module

 

This is also a cool feature of the BGM12 SiP modules. The antenna is really robust to the nearby materials like plastics.

 

Highlighted
Posts: 3
Registered: ‎08-14-2015

Re: Make it Small, Make it Fast, Make it First: Introducing the World’s Smallest Bluetooth Module

We also created whitepaper about Miniaturizing IoT Designs. This whitepaper explores the challenges that come with designing connected devices into increasingly smaller products, specifically antenna integration, and how system-in-package modules can help.

 

http://www.silabs.com/Support%20Documents/TechnicalDocs/miniaturizing-iot-designs.pdf