Reply
Posts: 11
Registered: ‎02-24-2017
Accepted Solution

Intensive communication application

Hi,

 

i work with WGM110 with BGlib API, 1.0.1 sdk version. It communicates with an extern MCU. The uart baud rate i choose is 625000 between MCU e the module.

there are a commands that needs information events. in this case my routine is:

-send the command

-wait the response,

-wait information events.

like as fdir command, fdir response, ffile and fready events.

While the module is sending me several ffile event messages, can i do some other operation with the module like as close an endpoint or some else command?

When the module is elaborating the events answer to the request, can i do something else with the module?

 

 

 

 

Posts: 2,058
Registered: ‎08-25-2015

Re: Intensive communication application

Hi,

 

Yes, you can, if the module can't accept your command for some reason you'll get an error code in the command response.

 

Regards,

Tiago

Posts: 11
Registered: ‎02-24-2017

Re: Intensive communication application

Thank you