Reply
Posts: 14
Registered: ‎01-31-2017

Fatal error: em_types.h

I am compiling the main IDAC demo file for EFM32 while attempting to port it onto EFR32 Blue Gecko using Gecko SDK suite but am having the following error- " fatal error: em_types.h: No such file or directory" (See attached)

 

Within the emstatus header file I can see the include statement for "em_types.h" but I cannot find that file anywhere within the SDK or online. Is there a suitable replacement I can use or better alternative?

Best,

 

Austin

Posts: 13
Registered: ‎12-04-2016

Re: Fatal error: em_types.h

I found it under Simplicity Studio (on Mac):

 

./developer/sdks/gecko_sdk_suite/v1.0/platform/middleware/glib/em_types.h