Reply
Posts: 2
Registered: ‎10-11-2017

Difference between BGM111 and BGM113??

I am using BGM113 module in my project. I want to know the difference between BGM111 and BGM113 including the specifications,features and compatibility.

Posts: 2,732
Registered: ‎09-01-2015

Re: Difference between BGM111 and BGM113??

BGM111 has higher TX power (max +8 dBm) compared to BGM113 (+3 dBm). In terms of Bluetooth features they are equivalent. 

 

Physically these two modules look a bit different. The BGM113 was designed to be footprint compatible with BLE113. Both BGM111 and BGM113 are based on the same SoC (EFR32BG1).

Posts: 2
Registered: ‎10-11-2017

Re: Difference between BGM111 and BGM113??

I also need to know the Difference between BGM111 and BGM121 and BGM113 and BGM11S??

Posts: 2,952
Registered: ‎08-25-2015

Re: Difference between BGM111 and BGM113??

Hi,

 

You sent the same question via private support ticket. Please do not duplicate your requests.

 

To help you in selecting the best module for your application please contact our distributors or sales in your region: https://www.silabs.com/buysample/pages/contact-sales.aspx

 

Regards,

Tiago