Reply
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> sjg
Posts: 38
Registered: ‎07-28-2016

Debugging an EFM32 product on a custom board

[ Edited ]

Hi,

 

Where does one find documentation for developing to a custom board in Simplicity?  I'm using the EFR32BG1B132F256GM489

 

Details:

I've started a new MCU project with kit:none, part: EFR32BG1B132F256GM489 SDK: bluetooth smart sdk ...

I chose the example project SOC Demo Health Thermometer

 

In the resulting .isc window, "general" tab, I verified the IAR toolchain.  In the "other" tab, I deselected using the hardware configurator (because that led to dead ends in all previous efforts), and then generated.

 

The subsequent build fails due to a missing bspconfig.h file.

I created one based upon an existing, and then created my own bsp_bcp.h file because that one caused trouble.

 

I'm now unable to find all the references in the stack code to bspconfig.h.  (I really don't understand THAT.)

 

Suggestions welcome.

 

(Sadly, I get significantly more responses when I rant than when I ask calmly.  It seems it should not be that way.)

 

Posts: 153
Registered: ‎01-06-2015

Re: Debugging an EFM32 product on a custom board

Hi,

 

Could try it with BLE SDK v2.0.0? It is much more flexible in case using custom hardware.

For this you need studio v4.

 

Cheers,

Balázs

 

 

Posts: 2
Registered: ‎10-06-2016

Re: Debugging an EFM32 product on a custom board

Will there ever be support for adding a custom board to Simplicity Studio? I am doing something similar with an EFR32 product on a custom board. The functionality of SS is very limited if it only allows for generating for predefined kits. I am using SS v4 and Blue SDK 2.0.0 and can't find any way to add a custom board. It is possible to use the sample and modify it for the custom board, but it would be much more efficient for other projects to allow a custom board definition in Simplicity Studio to test additional applications on the same board.