Reply
Posts: 5
Registered: ‎09-12-2017

Built-in self-test error 1121.8

I've been trying to debug the problem I posted about earlier and now I get the following error:

 

WRAP THOR AI (6.2.0 build 1121)
Copyright (c) 2003-2017 Silicon Labs Inc.
Built-in self-test error 1121.8 - please contact http://www.bluegiga.com/support
READY.

 


set
SET BT BDADDR 00:07:80:cc:7b:58
SET BT NAME DKWT32i
SET BT CLASS 600204
SET BT AUTH * 0000
SET BT IDENT BT:47 f000 6.2.0 Bluegiga iWRAP
SET BT LAP 9e8b33
SET BT PAGEMODE 4 2000 1
SET BT PAIR 00:12:6f:11:8f:d4 6cbfa973355871f6082ac5933637f2aa
SET BT PAIR 00:1f:82:3a:8f:f8 9a10b130f1eaabdc154ed951c281dd33
SET BT PAIR 4c:cc:34:31:a9:26 3f2febb98c4796cf6b07ddc052175b4f
SET BT PAIR 00:23:78:e8:ea:c7 453cd0b0d93d9547a76ca54270e2c1dd
SET BT POWER 6 6 6
SET BT ROLE 2 f 2580
SET BT SCO a 1 4d d 2 48
SET BT SNIFF 190 20 1 8 3c
SET BT SSP 3 0
SET BT MTU 667 672
SET CONTROL AUDIO INTERNAL INTERNAL EVENT
SET CONTROL BAUD 115200,8n1
SET CONTROL BIND 0 400 R VOLUME UP
SET CONTROL BIND 1 200 R VOLUME DOWN
SET CONTROL BIND 2 10 R AVRCP FORWARD
SET CONTROL BIND 3 8 R AVRCP PLAY
SET CONTROL BIND 4 1 R AVRCP PAUSE
SET CONTROL CD 00 0
SET CONTROL CODEC SBC JOINT_STEREO 44100 0
SET CONTROL CONFIG 0000 0000 0000 0d8b
SET CONTROL ECHO 7
SET CONTROL ESCAPE 43 00 1
SET CONTROL GAIN 8 8
SET CONTROL MICBIAS 8 2
SET CONTROL MSC DTE 00 00 00 00 00 00
SET CONTROL PIO 00 00 c6
SET CONTROL PREAMP 1 1
SET CONTROL READY 00
SET CONTROL RINGTONE &-5aaa;f:_6c-5a;f:_6c-5a_-6eee;f:_6c-5a;f:_6c-5a
SET CONTROL VREGEN 2 02
SET PROFILE A2DP SOURCE
SET PROFILE HFP Hands-Free
SET PROFILE HFP-AG HF Voice Gateway
SET PROFILE SPP Bluetooth Serial Port
SET PROFILE HSP-AG Voice Gateway
SET PROFILE AVRCP CONTROLLER 1f TARGET 0f
SET

 

Any hints as to what is causing this would be greatly appreciated! Thanks ahead of time,

Felix

Posts: 92
Registered: ‎06-05-2017

Re: Built-in self-test error 1121.8

Dear Flabelle,

 

this error means that CVC license is missing. In fact you are using CVC-enabled firmware. 

 

Regards,
Anna

Posts: 5
Registered: ‎09-12-2017

Re: Built-in self-test error 1121.8

Perfect, thank you!