Reply
Posts: 8
Registered: ‎03-09-2017
Accepted Solution

Buffer problem WF121A - Bgscript

Hi,

 

I have a problem with buffers.

I have initialized a buffer at the start of the script:   dim datatosend (8)

after at the event "system_boot" I use this buffer and I fill it with this code:    datatosend(0:8) = "Prova123"

 

When I try to use this buffer (for example reading it by USB endpoint with Bluegiga GUI - this is the command; call endpoint_send(3, 8, datatosend(0)),

only the first 4 bytes are filled with "Prov" the other bytes starting from the 4th byte are filled with \x04 \x00 \x00 \x00.

 

I try to use memcpy and other solution, but I reach the same result.

 

why?

Have I made a mistake?

Thank you

Highlighted
Posts: 8
Registered: ‎03-09-2017

Re: Buffer problem WF121A - Bgscript

After a deep-Search acitvity in the forum I have found the solution here:

http://community.silabs.com/t5/Bluetooth-Wi-Fi/BGScript-What-is-magic-required-to-access-strings-gre...

 

My mistake is to call the command:

endpoint_send(3, 8, datatosend(0))

instead of this one:

endpoint_send(3, 8, datatosend(0:8))

 

Thank you