Reply
Posts: 2,234
Registered: ‎09-01-2015

Bluetooth SDK 2.3.0 FAQ

[ Edited ]

This thread is dedicated to questions about the Bluetooth SDK 2.3.0 (released March 2017). The first post (the one that you are reading right now) is continuously updated so that it contains the latest status.

 

If your question is not specific to this BLE SDK version (2.3.0) then consider starting a new topic instead of replying to this topic.

 

NOTE: patch version 2.3.1 has been released, it replaces the 2.3.0.

 

Bluetooth SDK 2.3.0 FAQ

 

What's new in SDK 2.3.0?

 

New features include:

* Support for EFR32BG12 and EFR32MG12 product families

* Implementation for Bluetooth 5 2M PHY feature added. (EFR32BG12 and EFR32MG12 parts)

* Switched multiprotocol support

* GCC compiler support (Beta level)

* Bluetooth 5 Advertisement Sets

 

This is not a complete list. For more details, see the release notes.

 

For more information on the switched multiprotocol, see 

http://www.silabs.com/documents/public/user-guides/ug267-multiprotocol-user-guide.pdf

 

 

Where is the 2.3.0 SDK located, I can't find it?

 

The directory structure has changed starting from v2.3.0. Bluetooth SDK is now found under:

C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v1.0\

 

BGScript and NCP examples are found in:

...\gecko_sdk_suite\v1.0\app\bluetooth_2.3\

 

The libraries are in:

...\gecko_sdk_suite\v1.0\protocol\bluetooth_2.3\

 

In previous versions, the SDK was in:

C:\SiliconLabs\SimplicityStudio\v4\developer\stacks\ble\v2.1.1.0

 

GCC related questions

 

Note that GCC support is Beta level in SDK v2.3.0.

 

Is OTA supported in the 2.3.0 release with GCC?

 

Yes, OTA is supported. See following thread:

http://community.silabs.com/t5/Bluetooth-Wi-Fi/GCC-and-OTA/m-p/192115

 

Deprecated features

 

* BGScript support will be discontinued in the next major release

* BGscript is not supported with EFR32MG12,EFR32BG12 products (even in 2.3.0)

* most of the HW related commands / events have been marked as deprecated

 

For more details, see the release notes.

 

Known issues

 

Bad DC/DC configuration can cause unexpected resets when using maximum TX power (which is the default setting in most examples). => FIXED in SDK 2.3.1.

 

- Temporary workaround: lower the TX power with command gecko_cmd_system_set_tx_power

 


Update history, starting from the latest change:

* Apri 12 - Added note about 2.3.1 patch release that is now available

* April 3 - Added known issues  - unexpected resets due to bad DC/DC config

* March 16 - Added note about deprecated features 

 

 

Posts: 15
Registered: ‎11-11-2016

Re: Bluetooth SDK 2.3.0 FAQ

Hi all,

Please clarify question about Bluetooth 5 support and SDK 2.3.0:

 

Bluetooth 5 support is available just for new devices like EFR32BG12 and EFR32MG12?

Old devices like EFR32MG1P1 or EFR32BG1 ( Thunderboard sense and react)  can support Bluetooth 5 Advertisement Sets feature ?

Any Bluetooth 5 application development guide ?

Best regards,

Marcio

Posts: 2,234
Registered: ‎09-01-2015

Re: Bluetooth SDK 2.3.0 FAQ

Hi @msam,

 

the BT5 2M PHY is supported only on the new EFR32xG12 devices. 

 

The older EFR32MG/BG based products can support Advertisement sets and scan event reporting. Same applies to modules based on EFR32BG: BGM111, BGM113, BGM121.

 

Related topic:

http://community.silabs.com/t5/Bluetooth-Wi-Fi/New-Wireless-Gecko-SoCs-and-Bluetooth-Software-releas...

 

There is no BT5 application development guide at the moment. A knowledgebase article about how to use the BT5 advertising sets should be avaiable soon.

 

Posts: 6
Registered: ‎01-21-2017

Re: Bluetooth SDK 2.3.0 FAQ

Hi,

 

How and where do I find it? Is there a download? I have tried updating Simplicity Studio but I am still stuck with 2.1.1. I was going to download the Simplicity Studio installation again but it is the same version as I already have.

 

Thanks,

 

Rob

Posts: 2,234
Registered: ‎09-01-2015

Re: Bluetooth SDK 2.3.0 FAQ


rlkieth wrote:

Hi,

 

How and where do I find it? Is there a download?


There is no separate download, the new SDK is installed using Studio package manager. Try locating it under the SDKs, see screenshot below:

gecko-sdk.png

 

The version numbering can be a bit confusing: you need to install Gecko SDK Suite 1.0.0 which includes the latest BLE SDK v2.3.0. The wireless SDKs are organized like this because they share some common components like the emlib/emdrv libraries and Gecko bootloader.

Posts: 6
Registered: ‎01-21-2017

Re: Bluetooth SDK 2.3.0 FAQ

Thank for the reply.

 

I already have the Gecko platform 1.0.0.

 

I just found it under the Stacks tab. I am sure it wasn't there yesterday.

 

Cheers,

 

Rob

Highlighted
Posts: 5
Registered: ‎10-08-2015

Re: Bluetooth SDK 2.3.0 FAQ

 

It seems that 'Switched multiprotocol support' requires IAR toolchain run the demo?

Will this work with GCC in a future release?

 

Thanks

Posts: 5
Registered: ‎10-08-2015

Re: Bluetooth SDK 2.3.0 FAQ

Another quick question:

Seeing that BGScript is deprecated - Is the intention that these projects should be migrated to 'C' in the future?

Thanks!

Posts: 2,087
Registered: ‎08-25-2015

Re: Bluetooth SDK 2.3.0 FAQ

Hi,

 

That's your own choice, you can go with BGScript but that will lock you to the existing SDK release. If you want to use features which will be added in the next releases you'd have to migrate your app to C.

 

Regards,

Tiago