Reply
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> AMR
Posts: 1
Registered: ‎04-21-2017

BLE121LR

Hi there,

This is such a simple question but I've searched high & low to no avail...

I am using a host micro & just want to control the module using BGAPI.

The default UART parameters were easy to find:

UART baud rate: 115200
Hardware flow control: enabled
Data bits: 8
Parity: none
Stop bits: 1

But what are the default pins for RX, TX, RTS & CTS please?

Many thanks for your help.