Reply
Posts: 3
Registered: ‎01-24-2017

BLE112 & WF121 R&TTED and RED certification

Hello Together

 

Our Test lab told me, that the certification standard is changing this summer from R&TTED to RED.

Can you say me, if the both modules BLE112 and WF121 are re-certified with this standard?

I need it, because we plan a CE certification with a system, where these two modules are used.

 

BR

Tom

Highlighted
Posts: 2,817
Registered: ‎08-25-2015

Re: BLE112 & WF121 R&TTED and RED certification

Hi,

 

Our modules are undergoing testing at the moment for compliancy against the new standards. We expect to have the test reports during the first week of May and as soon as we have them we can share with customers upon request. Then we need to create the Declaration of Conformity documents and once that is ready we will put all the material available on our website.

 

Regards,

Tiago

Posts: 3
Registered: ‎01-24-2017

Re: BLE112 & WF121 R&TTED and RED certification

Hi Tiago

Thanks for the fast reply.

 

BR Tom