Reply
Posts: 8
Registered: ‎03-24-2017
Accepted Solution

BLE SDK 2.3.0 issues

Hi all,

 

I am working with a  Blue Gecko Wireless Starter Kit with a BGM121 module and Simplicity Studio V4. I have installed the latest BLE SDK 2.3.0, which now comes under the Gecko SDK Suite. However, I am having trouble running any of the available demos. The device seems to reboot after it receives the BGAPI command to start advertising.

 

Below, is the log that I got from BGTool when I programmed the module with the 'ncp-empty-target' demo, ran BGTool and clicked on the Advertise Start button.

 

10:35:22,0718 1 gecko_cmd_system_get_bt_address
10:35:22,0844 0 gecko_evt_endpoint_status endpoint: 3 (0x03) type: 0 (0x00000000) destination_endpoint: 4 (0x04) flags: 7 (0x07)
10:35:22,0866 0 gecko_evt_endpoint_status endpoint: 0 (0x00) type: 256 (0x00000100) destination_endpoint: -1 (0xffffffff) flags: 11 (0x0b)
10:35:22,0872 0 gecko_evt_endpoint_status endpoint: 31 (0x1f) type: 16 (0x00000010) destination_endpoint: -1 (0xffffffff) flags: 7 (0x07)
10:35:22,0885 0 gecko_evt_system_boot major: 2 (0x0002) minor: 3 (0x0003) patch: 0 (0x0000) build: 1981 (0x07bd) bootloader: 0 (0x0000) hw: 1 (0x0001)
10:35:22,0902 4 gecko_rsp_system_get_bt_address address:00:0b:57:25:b5:73
10:36:32,0425 1 gecko_cmd_le_gap_set_mode discover: 2 (0x02) connect: 2 (0x02)
10:36:32,0453 4 gecko_rsp_le_gap_set_mode result:0x0000 'Command completed succesfully'
10:36:33,0487 0 gecko_evt_endpoint_status endpoint: 2 (0x02) type: 1 (0x00000001) destination_endpoint: 9 (0x09) flags: 7 (0x07)
10:36:33,0493 0 gecko_evt_endpoint_status endpoint: 10 (0x0a) type: 0 (0x00000000) destination_endpoint: -1 (0xffffffff) flags: 11 (0x0b)
10:36:33,0502 0 gecko_evt_endpoint_status endpoint: 9 (0x09) type: 0 (0x00000000) destination_endpoint: 2 (0x02) flags: 7 (0x07)
10:36:33,0508 0 gecko_evt_endpoint_status endpoint: 4 (0x04) type: 0 (0x00000000) destination_endpoint: 3 (0x03) flags: 7 (0x07)
10:36:33,0514 0 gecko_evt_endpoint_status endpoint: 3 (0x03) type: 0 (0x00000000) destination_endpoint: 4 (0x04) flags: 7 (0x07)
10:36:33,0520 0 gecko_evt_endpoint_status endpoint: 0 (0x00) type: 256 (0x00000100) destination_endpoint: -1 (0xffffffff) flags: 11 (0x0b)
10:36:33,0526 0 gecko_evt_endpoint_status endpoint: 31 (0x1f) type: 16 (0x00000010) destination_endpoint: -1 (0xffffffff) flags: 7 (0x07)
10:36:33,0532 0 gecko_evt_system_boot major: 2 (0x0002) minor: 3 (0x0003) patch: 0 (0x0000) build: 1981 (0x07bd) bootloader: 0 (0x0000) hw: 1 (0x0001)

 

The issue does not seem to exist with SDK v2.1.1

 

Thank you,

Stathis

Highlighted
Posts: 5
Registered: ‎10-08-2015

Re: BLE SDK 2.3.0 issues

Apparently this is a small bug in 2.3.0 which they say will be patched soon.

 

This worked for us:

"Try lowering the transmit power with command cmd_system_set_tx_power before starting any advertising or scanning."

See the second post from JaakkoV in this thread:

http://community.silabs.com/t5/Bluetooth-Wi-Fi/Migrating-to-2-3-0/m-p/192180

 

Posts: 8
Registered: ‎03-24-2017

Re: BLE SDK 2.3.0 issues

Thank you RYan!

I reduced the TX power to 3 dBm and it seems to be working fine now.

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> Al
Posts: 2
Registered: ‎11-26-2016

Re: BLE SDK 2.3.0 issues

Any news on the update?

Also, on this version, when I use energy profiler on an exiting code running on the board, the system resets.