Reply
Highlighted
Posts: 9
Registered: ‎09-22-2015

BGM111 PWM?

Is there any information on how to use the hardware PWM outputs on the BGM111 or is something not available in the current firmware?

I tried using the hardware_timer_comparator function and is rejected by the compiler. 

Posts: 2,738
Registered: ‎09-01-2015

Re: BGM111 PWM?

Hardware PWM is not supported in current firmware.

Posts: 9
Registered: ‎09-22-2015

Re: BGM111 PWM?

Jaakov Thanks for your fast response. We are designing a new product using the BGM111 but we require the PWM outputs. At this moment we are getting by using an external PWM controller, but we would like to produce our first prototypes using only the BGM111 in early January. Do you think it would be possible to have a new SDK that supports PWM by then or should we use an external controller in our product? Of course that will make it more expensive because we are working in a very cost sensitive application. Any chance that we become some sort of beta tester to have early availability of the SDK in exchange of feedback?

Thanks!!! 

Posts: 2,738
Registered: ‎09-01-2015

Re: BGM111 PWM?

I will contact you using private message through our support system.

Posts: 1
Registered: ‎01-21-2016

Re: BGM111 PWM?

Hello everyone,

 

JaakoV, is there any new information available on PWM with BGM111 / BGScript?

 

PWM would make our job easier here Robot wink

 

Regards,

 

Tamas

Posts: 8
Registered: ‎06-13-2016

Re: BGM111 PWM?

Is there a workaround for "hardware_timer_comparator not recognized" in bgscript?

Posts: 7
Registered: ‎05-03-2016

Re: BGM111 PWM?

Are there any new information on supporting PWM in BgScript?