Reply
Posts: 2
Registered: ‎12-05-2016

BGM 113 - Testing Commands (test_dtm_rx) (BGScript)

Hello everybody,

I´m using the BGM113 Modul with BGScript.
Can anybody confirm that command test_dtm_rx(0, 1) is working correctly? The tx test mode is working fine but when I use the rx command my script freezes and I have to reboot the chip.

Thank you in advance!
Flow

Highlighted
Posts: 2,952
Registered: ‎08-25-2015

Re: BGM 113 - Testing Commands (test_dtm_rx) (BGScript)

Hi,

 

How are you reaching the conclusion that the script freezes? Can you attach your BGScript file?

 

Regards,

Tiago

Posts: 2
Registered: ‎12-05-2016

Re: BGM 113 - Testing Commands (test_dtm_rx) (BGScript)

Hi Tiago,

 

we solved the problem. Disconnect and then starting the test modes works fine.

 

Thank you!

 

Florian