Reply
Posts: 5
Registered: ‎09-04-2017

A2DP connection fails.

continue from

http://community.silabs.com/t5/Bluetooth-Wi-Fi/avrcp-connection-fails/m-p/208921


delete profile "AVRCP"

SET BT BDADDR 00:07:80:cb:55:c2
SET BT NAME WT32i-A
SET BT CLASS 280428
SET BT AUTH * 0000
SET BT IDENT BT:47 f000 6.2.0 Bluegiga iWRAP
.....
SET CONTROL VREGEN 1 00
SET PROFILE A2DP SOURCE
SET
reset
WRAP THOR AI (6.2.0 build 1118)
Copyright (c) 2003-2017 Silicon Labs Inc.
READY.
inquiry 3 name
INQUIRY_PARTIAL 00:1d:86:b0:cb:61 240404
INQUIRY 1
INQUIRY 00:1d:86:b0:cb:61 240404
NAME 00:1d:86:b0:cb:61 "NISSAN MJ116D" <---- my car navigation system
pair 00:1d:86:b0:cb:61
SSP CONFIRM 00:1d:86:b0:cb:61 285184 ?
ssp confirm 00:1d:86:b0:cb:61 ok
PAIR 00:1d:86:b0:cb:61 5 d1ed8652afb2337f39f4dd289d6d6746
PAIR 00:1d:86:b0:cb:61 OK
RING 0 00:1d:86:b0:cb:61 19 A2DP <---- connect from "NISSAN MJ116D"
RING 1 00:1d:86:b0:cb:61 19 A2DP
a2dp streaming start
A2DP STREAMING START 0
list
LIST 2
LIST 0 CONNECTED A2DP 48 0 0 93 0 0 00:1d:86:b0:cb:61 19 INCOMING ACTIVE SLAVE ENCRYPTED 0
LIST 1 CONNECTED A2DP 1017 0 0 92 0 0 00:1d:86:b0:cb:61 19 INCOMING ACTIVE SLAVE ENCRYPTED 0

 

I hear good music!!

 

close 0
A2DP STREAMING STOP 0
NO CARRIER 0 ERROR 0
NO CARRIER 1 ERROR 0
call 00:1d:86:b0:cb:61 19 a2dp <---- connect from WT32i
CALL 0
CONNECT 0 A2DP 19
NO CARRIER 0 ERROR a806 L2CAP_DISCONNECT_CONFIG_MISMATCH

 

I get the same error as before

 

Regards,
natsumi

Posts: 2,821
Registered: ‎08-25-2015

Re: A2DP connection fails.

Hi,

 

Why did you create a new thread instead of just continuing on the same thread? This doesn't make sense, it only makes it more difficult having to go back to another thread to see the initial information.

 

Regards,

Tiago

Posts: 5
Registered: ‎09-04-2017

Re: A2DP connection fails.

hi Tiago

 

sorry. I thought that if the thread is long it is not good.


Regards,
natsumi

Highlighted
Posts: 2,821
Registered: ‎08-25-2015

Re: A2DP connection fails.

Hi,

 

There's only 5 messages on that thread, that's far away from long. In any case, as long as the topic/issue remains the same it shouldn't be a problem. Jumping between threads creates additional problem of fragmenting the information.

 

Regards,

Tiago