WT11i/WT41 to WT11u/WT41u migration guide

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> bpienk on ‎02-13-2017 04:41 AM

On December 18th, 2015, Silicon Labs has announced discontinuance of WT11i and WT41 modules. EOL reason – components in BOM (power amplifier and antenna) became obsolete. However, there are new modules, which development has been finished – WT11u and WT41u.

 

WT11u is a drop-in, pin-to-pin compatible replacement for WT11i; WT41u is a drop-in, pin-to-pin compatible replacement for WT41. This concerns both its versions – internal “-i” and external “-e” antenna.

 

For both replacement variants:

  1. No hardware changes for PCB layout are needed. Footprint is exactly the same, ground planes extensions, clearance area, positioning at the PCB edge and other components around should remain the same. You may simply assemble the new module to your old PCB without any modifications.
  2. No software changes are needed – iWRAP software is exactly the same. This means that no modification for the host program is needed – all commands and functions will work in the same way as with the discontinued modules.
  3. Certification – similarly to the discontinued modules we will provide test reports and grants or declarations of conformity.

This means, that no additional effort (concerning both: hardware and software) is needed with the migration – you may simply take the new module (WT11u or WT41u), assemble it on your PCB and start the production.

 

The only difference is in iWRAP software version numbering in one case. Please take a look at the tables below, showing the difference:

 

Old WT11i part number

New WT11u part number

iWRAP software version

WT11I-A-AI4

WT11U-A-AI4

4.0.0 build 1101 (equal to build 317)

WT11I-A-AI5

WT11U-A-AI5

5.0.2 build 992

WT11I-A-AI56

WT11U-A-AI56

5.6.0 build 1022

WT11I-E-AI4

WT11U-E-AI4

4.0.0 build 1100

WT11I-E-AI5

WT11U-E-AI5

5.0.2 build 992

WT11I-E-AI56

WT11U-E-AI56

5.6.0 build 1022

 

Old WT41 part number

New WT41U part number

iWRAP software version

WT41-A-AI4

WT41U-A-AI4

4.0.0 build 1101 (equal to build 317)

WT41-A-AI5

WT41U-A-AI5

5.0.2 build 992

WT41-A-AI56

WT41U-A-AI56

5.6.0 build 1022

WT41-E-AI4

WT41U-E-AI4

4.0.0 build 1100

WT41-E-AI5

WT41U-E-AI5

5.0.2 build 992

WT41-E-AI56

WT41U-E-AI56

5.6.0 build 1022

 

 

Please also take a look at the table explaining the HCI firmware versions:

 

Old WT11i/WT41 part number

New WT11U/WT41U part number

HCI firmware version

WT11I-A-HCI21001

WT11U-A-HCI21001

4.0.0 build 1101 (equal to 317), HCI-USB

WT11I-E-HCI21001

WT11U-E-HCI21001

4.0.0 build 1101 (equal to 317), HCI-USB

WT41-A-HCI21001

WT41U-A-HCI21001

4.0.0 build 1101 (equal to 317), HCI-USB

WT41-E-HCI21001

WT41U-E-HCI21001

4.0.0 build 1101 (equal to 317), HCI-USB

 

Please be informed, that not all legacy firmware versions have been ported to support new modules, including regular releases and the ones created as customer builds. You might like to ask for a new custom part with your own custom or legacy firmware; for this purpose, please contact the Silicon Labs Support via the support portal at:

http://www.silabs.com/support/Pages/default.aspx

 

Please also remind, that any firmware is in the most part of it backwards compatible.