Creating projects for EFR32BG on a custom board

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Legend Employee</font></font> </a> tmonte ‎12-13-2016 05:34 AM - edited ‎12-13-2016 05:40 AM

1. On the Solutions tab of Simplicity Studio Launcher press Add Devices, type your device name and select it from the drop down list. It's important that you select a device listed under Parts and not under Kits or Boards

 

1.png

 

2. With your device selected on the Custom Solution tree press New Project

 

2.png

 

3. Select Silicon Labs Bluetooth Smart Framework and press Next

 

4. Select the stack version that you want to use and press Next

 

5. Select the example that you want to start from and press Next. Typically you will want to start from the SOC - Empty example

 

4.png

 

6. Select your project name and location and press Next

 

7. On the final window confirm that the part number is correct and press Finish which will then automatically open Simplicity IDE

 

5.png

 

Comments
by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> bcm
on ‎04-30-2017 08:31 AM

Nice tutorial!

 

Does this apply to creating a NCP bgapi project as well.  By creating a project it will allow the use of the GATT configurator for this type of project any other benifits?

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja Employee</font></font> </a> JoonasI
on ‎06-27-2017 03:21 AM

Since the deprecation of BGBuild as a tool to create NCP images starting from the 2.4.0 software release, this is the recommended way to create NCP projects. Alternatively, projects can be created using IAR or GCC.