BGM113 Reset Pull-up Pin Strength

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> PhillipB on ‎07-05-2017 02:55 PM

Question

What is the strength of the internal pull up on the BGM113 RESETn pin?

Answer

The internal pull-up on the BGM113 reset line (RESETn) is the same as those present on other GPIO pins, and is specified in the BGM113 Data Sheet by the "I/O pin pull-up resistor" (RPU) parameter in Table 4.20 "GPIO" (of section 4.1.11 GPIO).  RPU is specified as 30/43/65 kOhm (min/typ/max) in the revision 1.00 data sheet.