Reply
Posts: 11
Registered: ‎09-28-2017

f300

Can someone tell me if this is a C8051F300

 

F300

E26M

649+

 

What do the numbers under F300 mean?

Posts: 343
Registered: ‎03-03-2015

Re: f300

I can't read the package markings on the picture you took.  If it is a 'F300 the numbers after are a trace code (to indicate which lot it came from) and a date code.  649 would mean the 49th week of 2006.

 

Regards,

Joe

Posts: 11
Registered: ‎09-28-2017

Re: f300

Joe, Thanks for your Response.

Here is a better picture! It is a

Portable 125KHz RFID Reader & Writer Duplicator Copier Programmer Device

 

I heard the F300 in these units are not stable. Is there a way I can read the F300 and save it to file.

In case I need it in the future.  I am still reading more info.  I bought this unit which has not yet arrived.

C8051F MCU Emulator U-EC6 USB Debug Adapter JTAG/C2 Mode with Cable

Is this Debugger used to read and write F300?

Once again thanks for your Time!

 

 

Posts: 343
Registered: ‎03-03-2015

Re: f300

[ Edited ]

The F300 uses the C2 protocol.  The debugger you have will work, connect to the C2CK and C2D pins (see the pinout on page 28 here: https://www.silabs.com/documents/public/data-sheets/C8051F30x.pdf ).  You will only  be able to retrieve the firmware from the device if it is not locked, and in most commercial products, the microcontroller is locked.  You could ask the manufacturer if they will send you a binary of their code, but I don't know if they will.

 

Regards,

Joe

Posts: 8,172
Registered: ‎08-13-2003

Re: f300

 You could ask the manufacturer if they will send you a binary of their code, but I don't know if they will.

if they are willing to send, why not ask for the source?

erik
Posts: 343
Registered: ‎03-03-2015

Re: f300

You can ask for anything you want, but I'd think most manufacturers would be more reluctant to send source than a binary image.  Of course, the point of locking the device is so that users can't get access to it, so if they did that, they may not want to share the code.

 

Regards,

Joe

Posts: 11
Registered: ‎09-28-2017

Re: f300

Joe, once again thanks for response.  Your link you posted is Dead!.

I will google for it. Thanks.

 

Posts: 343
Registered: ‎03-03-2015

Re: f300

The closing parenthesis got added to the url accidentally, I've edited the post to fix it.  The URL is: https://www.silabs.com/documents/public/data-sheets/C8051F30x.pdf

 

Regards,

Joe

Posts: 11
Registered: ‎09-28-2017

Re: f300

I have 2 of these Devices!  They are like a 10 dollar unit. And so many Distributors in China

selling. Most of them say they are Manufacturers. Once I get my Debugger and Learn how

to use it, without Destroying the on Board F300.

Posts: 11
Registered: ‎09-28-2017

Re: f300

Thanks Joe!

Posts: 11
Registered: ‎09-28-2017

Re: f300

Question do you use the Simplicity Studio to read/write f300 . I know it uses the C2 Protocol. with 2 pins attached.

Posts: 11
Registered: ‎09-28-2017

Re: f300

I think I bought the Wrong Adapter?

Posts: 2,380
Registered: ‎10-14-2014

Re: f300

Posts: 11
Registered: ‎09-28-2017

Re: f300

Delu, thanks for Link. However I do not have sufficient privideges to access.