Reply
Posts: 25
Registered: ‎03-24-2017

USB mass storage device on nand flash

Hi,

 

I am trying to connect a NAND flash memory to 

Posts: 25
Registered: ‎03-24-2017

Re: USB mass storage device on nand flash

Hi,

 

I am trying to connect a NAND flash memory to  C8051f320 or C8051f340 to Write and read data from PC to Nand flash through USB connection. I find out that there is a firmwhare from Silabs which can be used to know the SD card from windows as a flash drive. Kindly help if I can customize the library (low levels) so that I can use a nand flash instead of SD card with the firmware.

 

Regards,

Raja