Reply
Posts: 8,015
Registered: ‎08-13-2003

TPS2104DBVR:Obtainable positive and negative output of the ideal diode circuit ??? Why ?

Posts: 16
Registered: ‎02-16-2017

Re: TPS2104DBVR:Obtainable positive and negative output of the ideal diode circuit ??? Why ?

I can tell you that you don't have the right to remove others' posts as a spam and that is not a responsible behavior.

Posts: 434
Registered: ‎01-18-2004

Re: TPS2104DBVR:Obtainable positive and negative output of the ideal diode circuit ??? Why ?


maryzhu wrote:

I can tell you that you don't have the right to remove others' posts as a spam and that is not a responsible behavior.


The post was clearly off topic. It had nothing to do with a Silicon Labs 8-bit microcontroller, or indeed any SiLabs device, and as such was properly moved.

Posts: 2,887
Registered: ‎02-07-2002

Re: TPS2104DBVR:Obtainable positive and negative output of the ideal diode circuit ??? Why ?

Further, since erikm has gained the state of moderator, that means exactly that he does have that right.

 

But as I have said before, don't feed this troll. And as far as I'm concerned he can be blocked.

Posts: 8,015
Registered: ‎08-13-2003

Re: TPS2104DBVR:Obtainable positive and negative output of the ideal diode circuit ??? Why ?

I do not think the comment was specifically directed at me, I think it meant "nobody has the right to delete what i post wherever I post it"

erik