Reply
Highlighted
Posts: 56
Registered: ‎03-22-2017
Accepted Solution

IDE licensing

Installed IDE on a new laptop, hitting the size limit. Went and got the license (AN104) and installed it in Keil uVision, but no joy. Still getting the error:

Program Size: data=47.0 xdata=140 const=0 code=5069
*** ERROR L250: CODE SIZE LIMIT IN RESTRICTED VERSION EXCEEDED
LIMIT: 0800H BYTES

 

Verified that uVision is happy with the license, no errors or messages there.

How to fix?

Thanks

 

Posts: 8,172
Registered: ‎08-13-2003

Re: IDE licensing

[ Edited ]

Installed IDE

 

IDE: "classic IDE" or Simplicity Studio?

erik
Posts: 56
Registered: ‎03-22-2017

Re: IDE licensing

Classic - the old one.

Posts: 8,172
Registered: ‎08-13-2003

Re: IDE licensing

someone with a similar problem found out he had 2 copies of Keil, do you?

erik
Posts: 56
Registered: ‎03-22-2017

Re: IDE licensing

Thanks, that helped me fix it. I have two paths on my HD. One is "Keil", the other is "Keil_V5". Both have uVision 5 in them. Both of those had licenses entered.

My IDE toolchain was pointing to the "Keil" path, so I changed it to "Keil_V5", and then it compiled okay.

No idea how both versions of Keil exist. I suspect that the old one was installed with IDE, and then when I installed SS4, maybe that installed the newer Keil_V5.

Working now, so thanks again.

Posts: 8,172
Registered: ‎08-13-2003

Re: IDE licensing

since it solved the issue, please mark it as a solution

erik