Reply
Highlighted
Posts: 3
Registered: ‎04-06-2017
Accepted Solution

Flash utilities running from command line to program C8051F410

Hi,

 

Could anyone please specify the command line arguments needed to run flashutils from command line ? or even IDE not the studio from command line ?

 

I am not able to find the options with command FlasUtils and IDE.

 

Thanks

Posts: 2,810
Registered: ‎02-07-2002

Re: Flash utilities running from command line to program C8051F410

Have you tried to run it with no parameters? Or with -h, --help, /?.

And remember you even get the sources for this program, so you could inspect them as well.

Posts: 1,733
Registered: ‎10-14-2014

Re: Flash utilities running from command line to program C8051F410

@mvivek16

I think you are asking how to use the FlashUtilCL.exe command line tool.

In addition to the method mentioned by @vanmierlo, I think you could see an readme.txt file after install the package. there is explanation on what the meaning of the argument.

WeiguoLu