Reply
Posts: 10
Registered: ‎03-19-2014

FLASH utility source code not compiled in VC++

Hi 

i am getting below log while  compiling, so please help me make it run

 

1>------ Build started: Project: downloader, Configuration: Debug Win32 ------
1>Compiling...
1>cl : Command line error D8030 : INTERNAL COMPILER ERROR in ''
1> Please choose the Technical Support command on the Visual C++
1> Help menu, or open the Technical Support help file for more information
1>Creating browse information file...
1>Microsoft Browse Information Maintenance Utility Version 9.00.21022
1>Copyright (C) Microsoft Corporation. All rights reserved.
1>BSCMAKE: error BK1506 : cannot open file '.\Debug\downloader.sbr': No such file or directory
1>Build log was saved at "file://C:\SiLabs\MCU_2_3\Utilities\FLASH Programming\Static Programmers\Windows Console\FlashUtil Source Files\Debug\BuildLog.htm"
1>downloader - 2 error(s), 0 warning(s)
========== Build: 0 succeeded, 1 failed, 0 up-to-date, 0 skipped ==========

Posts: 3,100
Registered: ‎02-07-2002

Re: FLASH utility source code not compiled in VC++

I suggest to first try to clean and rebuild the project. A .sbr file is an intermediate file which it should be able to regenerate.

Posts: 10
Registered: ‎03-19-2014

Re: FLASH utility source code not compiled in VC++

Thanks vanmierlo,

i cleaned the project first and then Compiled after that i got mentioned problem

at the first step only i am getting following error. Smiley Sad

 

 cl : Command line error D8030 : INTERNAL COMPILER ERROR in ''