Reply
Posts: 55
Registered: ‎10-25-2016

EFM8UB11F16G Uart baud rate

i am working with EFM8UB11F16G Controller ,default UART baud rate in simplicity studio is 115500 ,do any one know how to change baud rate to 9600???

 

Posts: 1,733
Registered: ‎10-14-2014

Re: EFM8UB11F16G Uart baud rate

you could easily use the configurator to set baud rate. as far as i remember the UART EFM8UB example code provide a configurator file.
WeiguoLu
Posts: 7,951
Registered: ‎08-13-2003

Re: EFM8UB11F16G Uart baud rate

,do any one know how to change baud rate to 9600???

 

yes, the reference manual "knows"

erik
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> jmg
Posts: 1,107
Registered: ‎04-27-2004

Re: EFM8UB11F16G Uart baud rate


pradnya wrote:

i am working with EFM8UB11F16G Controller ,default UART baud rate in simplicity studio is 115500 ,do any one know how to change baud rate to 9600???

 


 If you mean change the Simplicity Studio Baud Rate, my understanding that extension is real close now...

 My info from SiLabs was the WSTK just has Baud and Handshake added (9600...921600) in Dec, and the STK (EFM8xx) was following that..

 

Highlighted
Posts: 7,951
Registered: ‎08-13-2003

Re: EFM8UB11F16G Uart baud rate


 If you mean change the Simplicity Studio Baud Rate

 

good catch, two of us missed that one

erik