Reply
Posts: 9
Registered: ‎10-12-2016

Does AN107 also apply to other 8051 products?

I am looking for an AN describing how to use the PCA0CPn in 16 bit PWM mode with more than one output. AN107 seems to be the one - but it says it only applies to C8051F000, C8051F001, C8051F002, C8051F005, C8051F006, C8051F010, C8051F011, and C8051F012.

 

Does AN107 also apply to the 8051F501? If not, is there another app note I should be looking at?

Thanks in advance -

Posts: 2,321
Registered: ‎10-14-2014

Re: Does AN107 also apply to other 8051 products?

@dnmeeks

As far as I know the PCA module should use similar architecture for C8051 device.

I am not sure about your detailed requirement. the different channels (capture/compare) could be routed to different external pin(CEXx).

: My views are my own and do not necessarily represent the views of Silicon Labs

WeiguoLu
Posts: 8,134
Registered: ‎08-13-2003

Re: Does AN107 also apply to other 8051 products?

for all PCA stuff

 

PCA cookbook http://application-notes.digchip.com/027/27-46415.​pdf

 

the difference in the SILabs PCA's from the original Intel are nominal;

 

re the AN the architecture of the derivatives 8051f 00-02 is different from the architecture of the deviates -03-09 & EFM

erik