Reply
Posts: 60
Registered: ‎10-25-2016

CPU core could not start

when i connected EFM8UB evaluation and try to  run sample code i am getting

 

J-Link V6.10G Error

communication timed out: Requested 4 bytes,received 0 bytes

could not start CPU Core(errorcode:-1)

how to overcome from these problem???

Posts: 466
Registered: ‎02-21-2014

Re: CPU core could not start

Could you check the power switch on the STK to make sure it's set to 'AEM'?

Posts: 60
Registered: ‎10-25-2016

Re: CPU core could not start

yes it is set to AEM Mode ,actually device is connected but when i upload code in evaluation board that time error is coming ,do u think some file is missing in simplicity studio or problem in evaluation board??/

Posts: 182
Registered: ‎07-12-2016

Re: CPU core could not start

hi @pradnya,

 

Did you even try to upgrade the J-Link FW of the evaluation board ? And how about the FW version of your board.

Do you have any other boards on hand, and how about the performance of others ?

 

Untitled.png

 

Thanks

Posts: 466
Registered: ‎02-21-2014

Re: CPU core could not start

Could you also try erasing the device in the flash programmer after updating the kit firmware (if that doesn't work) ?

 

erase.png

 

If neither of those work, I would open a support ticket to see if we can get your kit replaced. It might also be helpful if we could get your kit to see what's gone wrong with it.

 

 

Highlighted
Posts: 60
Registered: ‎10-25-2016

Re: CPU core could not start

My Board is EFM8UB1 Universal bee kit (ST2000A)

Curently i am using EFM8UB11FI6G(24 pin)on custom board ,i have pcb ,when i connect my custom board everything is working fine and when i connect the evaluation board it is showing error cpu core not detected

Posts: 60
Registered: ‎10-25-2016

Re: CPU core could not start

@BrianL when i try to erase it is showing same error  ,communication timed out

Posts: 466
Registered: ‎02-21-2014

Re: CPU core could not start

And your kit is in Debug Mode: MCU when you attempt to connect to the chip on the kit?

 

MCUDebugMode.png

Posts: 2,321
Registered: ‎10-14-2014

Re: CPU core could not start

Do you still have this issue, this is very strange. Do you mean you only have this issue with th EFM8 UB1 STK and don't have any problem on your own board? What debugger you are using to connect your own customized board?
WeiguoLu