Reply
Posts: 49
Registered: ‎07-31-2011

C8051F340 and COM port over USB on Windows10

I'm searching over the forum and found HID drivers, examples, and some USBXpress example but not work by me as simple serial COM port!

Can you suggest me simple tutorial and sw download links how C8051F340 connect with PC (Win10) as serial port over integrated USB port?!

So...this example must work with any terminal program on windows which support serial ports!

 

Thanks!

Posts: 182
Registered: ‎07-12-2016

Re: C8051F340 and COM port over USB on Windows10

hi @js1234,

 

If you download the latest SDK, the example can be found under the folder as below.

C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\8051\v4.0.6\examples\C8051F340DK\USB\VCPXpress\C8051F340_VCPXpress_UsbToUart

 

Thanks

Posts: 49
Registered: ‎07-31-2011

Re: C8051F340 and COM port over USB on Windows10

WOW! Robot Happy working! Robot Happy

THANKS!

 

p.s.

on SDK 4.0.7 on my PC:

C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\8051\v4.0.7\examples\C8051F340DK\USB\VCPXpress\C8051F340_VCPXpress_UsbToUart