Reply
Posts: 6
Registered: ‎04-11-2014

C8051F020 calculator

I have built a basic scientific calculator using the C8051F020, an LCD and a keypad (hobby project). Code and schematics can be found here:

 

http://www.southerncrossmicro.com/pages/MTEST.html

 

 

Posts: 344
Registered: ‎02-26-2013

Re: C8051F020 calculator

@Danno, thanks for sharing your work!

Highlighted
Posts: 6
Registered: ‎04-11-2014

Re: C8051F020 calculator

Here is a video of two calculators I have built, one using a C8051F020 and LCD and the other a C8051F120 and GLCD:

 

https://www.youtube.com/watch?v=p7MBGPf2i6E

 

For the C8051F020 I wrote the code in C and used the floating point library. For the C8051F120 I wrote assembly routines to add, subtract, multiply and divide two 16-bit integers. 

 

I would like to write C code to perform arithmetic operations on decimals and build up a scientific calculator that eventually does powers, trigonometric functions etc. 

 

This is a hobby project and I want to write all of the routines and not depend on libraries. Does anyone know of resources that would help me with this? I have read Clive Maxfield's excellent "How computers do math" that explains integer math and am now looking for material on floating-point routines. 

This video shows two calculators I made using an 8051 microcontroller, 4x4 matrix keypad and a character LCD (for the first calc) and a graphical LCD (for the second calc). For instructions on how to build these calculators, visit www.southerncrossmicro.com