Reply
Posts: 10
Registered: ‎05-05-2016
Accepted Solution

Bootloader for C8051F3XX

We use C8051F3XX in various products, all w/ USB.

I would like to use a bootloader for firmware upgrades.

I skimmed AN200, AN533.

It looks like there has to be a separate MCU (Master Programmer)??

Is there any way to put the bootloader on the one and only MCU on my board, and comm directly w/ PC over USB?

Thanks,

Emmett

Posts: 7,815
Registered: ‎08-13-2003

Re: Bootloader for C8051F3XX

Is there any way to put the bootloader on the one and only MCU on my board, and comm directly w/ PC over USB?

 

sure, that is the usual meaning of a bootloader.  What probably is confoosing you is that a bootloader does NOT use the EC2 pins/method

erik
Posts: 10
Registered: ‎05-05-2016

Re: Bootloader for C8051F3XX

Thanks for the reply.

What had me concerned was the statement in AN533, page 1:

"The current release of the modular bootloader framework supports option 2 only"

Option 2 being the master programmer method.

 

I am now following AN200.

Is this the best path to follow?

 

Thanks,

Emmett

Highlighted
Posts: 7,815
Registered: ‎08-13-2003

Re: Bootloader for C8051F3XX

I am now following AN200.

Is this the best path to follow?

sounds like a decent choice

erik
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> jmg
Posts: 1,035
Registered: ‎04-27-2004

Re: Bootloader for C8051F3XX


 

I am now following AN200.

Is this the best path to follow?


 

 

You could also look at the EFM8UB2 USB bootloader ? (or even move to the EFM8UB2 entirely, and make use of the inbuilt bootloader )