Variable overlay thickness for capacitive sensors

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> jstine on ‎03-31-2017 10:31 AM

Question

How can I handle capacitive sensors with varying overlay thickness in cslib?  Is it possible to set different touch deltas for different sensors?

Answer

It is not possible to set touch deltas on a per-sensor basis in the current version of cslib.  However, you can alter the drive strength for each channel to compensate for different overlay thickness.