Route multiple analog peripheral input to same port pin

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Master Employee</font></font> </a> delu on ‎07-04-2017 03:15 AM

Question

Could we route multiple analog peripherals input to same port pin?

For EFMLB1 device, when I use configurator to route ADC and CMP0 to P1.7 but it reports error.

Answer

Yes, this is possible.

Though configurator reports error, you could manually modify the code.

We don't have plan to make change to the configurator to suppress this error.