How to use Flash Utility Command-line Tool for Multi-Device JTAG Chain Programming

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Jiehui ‎08-22-2017 11:35 PM - edited ‎08-30-2017 04:05 AM

AN134 describes the Multiple-Device JTAG Chain configuration in the legacy Silicon Labs IDE.

 

Here is an example on how to use the Flash Utility command-line tool for Multi-Device JTAG programming using Silicon Labs USB Debug Adapter (UDA). For more details on these commands, Please refer to the readme.txt included in the command-line tool.

 

 Multi-JTAG.png